Search FAQs
How is the ATV212 set for HMI controls for both RUN/STOP and speed reference?
Issue:
How is the ATV212 set for HMI controls for both RUN/STOP and speed reference?
Product Line:
Altivar 212
Environment:
All models
Cause:
Control for VFD to be from the HMI
Resolution:
There are several options.
1) Put the VFD in Local Mode by pressing the LOC/REM button on the integral keypad, or the F4 button on the remote keypad. Indicators for Local Mode are the green LED is ON for LOC/REM, or LOC is displayed above the F1 button.
2) Keep the VFD in Remote Mode and set CMOd=1 and FMOd=3
Both of these options apply for integral keypad or remote keypad control.
How is the ATV212 set for HMI controls for both RUN/STOP and speed reference?
Product Line:
Altivar 212
Environment:
All models
Cause:
Control for VFD to be from the HMI
Resolution:
There are several options.
1) Put the VFD in Local Mode by pressing the LOC/REM button on the integral keypad, or the F4 button on the remote keypad. Indicators for Local Mode are the green LED is ON for LOC/REM, or LOC is displayed above the F1 button.
2) Keep the VFD in Remote Mode and set CMOd=1 and FMOd=3
Both of these options apply for integral keypad or remote keypad control.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: