{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How is a remote fault reset contact added to an ATV312?

Article available in these languages: Spanish

Issue:
Installing a remote fault reset contact on an ATV312

Product Line:
Altivar 312

Environment:
All

Cause:
Manual fault reset

Resolution:
Wire a normally-open contact to 24V and LIx (the logic input to be used as fault reset)
In the FLt menu, set rSF to LIx
In the event the drive faults, manually closing the contact will reset certain faults

Note: Not all drive faults can be reset this way. Safety-related faults must be reset by power-cycling the drive. Consult the ATV312 Programming Manual for lists of faults that require a power cycle to reset.


Schneider Electric Nigeria