Issue:
Setting up the ATV212 for a run permissive
Product Line:
ATV212 S-Flex212
Environment:
All models and serial numbers
Cause:
N/A
Resolution:
Wire a dry contact to P24 and a logic input (F, R, or RES). Program F110 = 0 to remove the always active run permissive. Then set the logic input = 1 to assign run permissive to it (F111=1, F112=1, or F113=1). When the remote contact is closed, the drive is permitted to run and is ready for a run command.
Setting up the ATV212 for a run permissive
Product Line:
ATV212 S-Flex212
Environment:
All models and serial numbers
Cause:
N/A
Resolution:
Wire a dry contact to P24 and a logic input (F, R, or RES). Program F110 = 0 to remove the always active run permissive. Then set the logic input = 1 to assign run permissive to it (F111=1, F112=1, or F113=1). When the remote contact is closed, the drive is permitted to run and is ready for a run command.
Released for:Schneider Electric Nigeria