{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
On an ATV312, is drive protection compromised when Output Phase Loss is disabled (OPL = NO)?

Article available in these languages: Spanish

Issue:
Setting OPL = NO on an ATV312

Product Line:
Altivar 312

Environment:
All

Cause:
Need to turn off OPL, possibly for testing purposes

Resolution:
OPL is an output phase loss detection.  This feature is intended to protect the motor from imbalanced current or single phasing.  Disabling the feature has no adverse affect on the drive; however, it should only be disabled for testing the drive without a motor connected or if drive is installed with a full voltage bypass.


Schneider Electric Nigeria