{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the ATV212 and ATV312 drives have output phase loss protection?
Issue:
Output phase loss protection on ATV212 and ATV312 drives

Product Line:
Altivar 212, Altivar 312

Environment:
All models, all serial numbers.

Cause:
Protection from the loss of an output phase.

Resolution:
Both the ATV312 and ATV212 have output phase loss protection.

Output phase protection can be deactivated on both of these drives if needed for testing purposes:
For the ATV312 go to FLT > OPL and change from YES to NO to deactivate phase protection.
For the ATV212, press Mode until you see AUF, then scroll down to F - - - and hit Enter.  Scroll down to F605 and change to '0' to deactivate.

Schneider Electric Nigeria

Do the ATV212 and ATV312 drives have output phase loss protection?
Issue:
Output phase loss protection on ATV212 and ATV312 drives

Product Line:
Altivar 212, Altivar 312

Environment:
All models, all serial numbers. 

Cause:
Protection from the loss of an output phase. 

Resolution:
Both the ATV312 and ATV212 have output phase loss protection. 

Output phase protection can be deactivated on both of these drives if needed for testing purposes:
For the ATV312 go to FLT > OPL and change from YES to NO to deactivate phase protection.
For the ATV212, press Mode until you see AUF, then scroll down to F - - - and hit Enter.  Scroll down to F605 and change to '0' to deactivate.

Schneider Electric Nigeria

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:
move-arrow-top