{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What features are lost by adding the LonWorks option card VW3A21212 to the Altivar ATV212 drive?

Issue:
Some features are lost if the optional LonWorks card is added to the ATV212 drive.

Product Line:
Altivar ATV212 and ATV21

Environment:
All

Cause:
Updating to the LonWorks option card you will loose some features on the drive.

Resolution:
If the optional LonWorks card replaces the standard card, the following features are lost:

  • VIA 4 to 20mA input will be removed
  • FM analog output will be removed
  • RYA and RYC relay output will be removed.
This is also option B06 on the S-Flex enclosed package drives.

Schneider Electric Nigeria