{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Legacy APC Refrigerant Charge

Issue:
Legacy APC Refrigerant Charge

Product line:
Legacy, Airflow, AFX, CCT, CM, TC

Environment:
All Models

Cause:
Factory Refrigeration Charge

Resolution:
Please note that the charge amounts below are "total" for the unit(s) Som units below have two independant circuits.

R-22 Factory Charged

Air

W/G

CCT-6 W/G

8.1

CM15

56 ozs

47 ozs

CCT-8 W/G

12

CM20

63 ozs

54 ozs

CCT-10 W/G

13

CM25

70 ozs

63 ozs

CCT-15 W/G

24

CM40

101 ozs

84 ozs

CCT-20 W/G

27

CM65

170 ozs

120 ozs

CCT-24 W/G

31

CCT-30 W/G

70

TC-2 W/G

5

TC 3 W/G

4lbs, 13 ozs

TC-5 W/G

8.5

TC-8 W/G

11

TC-10 W/G

11

AFX-106 W/G

13

AFX-108 W/G

18

AFX-210 W/G

23

AFX-212 W/G

23

AFX-214 W/G

23

AFX-218 W/G

23

AFX-320 W/G

44

AFX-326 W/G

44

AFX-328 W/G

57

All charges are approximate, may vary +/- 5 lbs.

Schneider Electric Nigeria

Explore more
Range:
Uniflair Room Cooling Accessories
Explore more
Range:
Uniflair Room Cooling Accessories
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.