{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to set a start/stop on LI1 and a LSP speed on ATV312 drive?
Issue:
Use start/stop on LI1 and set a LSP speed on ATV312 drive.

Product Line:
ATV31 and ATV312
Environment:
All models and serial numbers

Cause:
None
Resolution:
Enter the motor parameters in the DRC menu (BFR: UNS, FRS: NCR: NSP).
Wire a start/stop contact between LI1 and +24V.  Set low speed in the SET menu with parameter LSP.  Assign the value in frequency.

Schneider Electric Nigeria