{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to assign a logic input to freewheel stop on Altivar 61 and 71?

Issue:
Freewheel stop assignment on ATV61/71.

Product Line:
Altivar 61 and 71

Environment:
All models and serial numbers

Cause:
None

Resolution:
Go to Drive menu, 1.7 Application function menu, and assign Freewheel Stop assignment to a logic input (LIx) as desired.

NO.        MENU                              SUB-MENU        CODE   ADJUST    DESCRIPTION
1.7    APPLICATION FUNCTION    STOP CONFIG.    Nst      LIx            Freewheel stop input

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: