{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How do you wire and program an ATV31 or ATV312 to follow an external 0-10vdc speed pot on Analog Input 1 and use the logic inputs for starting and stopping?
Issue:
ATV31/312 set up to follow an external 0-10vdc speed pot on AI1 and use the logic inputs for starting and stopping.

Product Line:
Altivar 31 and 312

Environment:
All models in range.

Cause:
Pot for speed control or 0-10v logic input for speed control.

Resolution:
Wiring:
Wire your external pot to AI1 com and +10vdc. (wiper wire on AI1)
Wire your Start forward command between LI1 and +24vdc.

Programming:
Step 1: Go into the CTL menu enter
Step 2: Set Fr1 to AI1

Schneider Electric Nigeria

Attachment(s)
Program BBV46385_03 ATV312.pdf [2.6 MB]