Issue:
How can I change the motor direction in drive mode and bypass mode?
Product Line:
All enclosed with a bypass option
Environment:
All
Cause:
Motor is running in the correct direction in drive mode and reverse in bypass mode.
Resolution:
-If the motor runs the correct direction from the drive but the wrong direction in bypass, swap any 2 incoming power leads into the cabinet.
-If the motor runs the correct direction in bypass but the wrong direction from the drive, swap any 2 motor leads coming out of the drive on UVW
or you can change the programming phase rotation in menu 1.1 simple start menu from ABC to ACB.
How can I change the motor direction in drive mode and bypass mode?
Product Line:
All enclosed with a bypass option
Environment:
All
Cause:
Motor is running in the correct direction in drive mode and reverse in bypass mode.
Resolution:
-If the motor runs the correct direction from the drive but the wrong direction in bypass, swap any 2 incoming power leads into the cabinet.
-If the motor runs the correct direction in bypass but the wrong direction from the drive, swap any 2 motor leads coming out of the drive on UVW
or you can change the programming phase rotation in menu 1.1 simple start menu from ABC to ACB.
Released for:Schneider Electric Nigeria