{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is EPH1 fault on ATV212?

Issue:
EPH1 fault on ATV212

Product Line:
ATV212, ATV21

Environment:
All models and serial numbers

Cause:
External or internal

Resolution:EPH1 is an input phase loss.

Verify the wiring connections on all three phases coming into the drive (R/L1-S/L2-T/L3).
Measure line to line voltages to make sure they are all present and equal phase to phase.
To clear the fault, cycle power. Turn off the line voltage until the display goes off.  Then turn the voltage back on.

Schneider Electric Nigeria