{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How do I change from ramp stop to freewheel stop on the ATV61 and ATV71 drives?
Issue:
Programming Freewheel Stop on Altivar 61 & 71 Drives

Product line:
ATV61, ATV71

Environment:
All models, all serial numbers

Cause:
Need to change the stop type to support application.

Resolution:
  • Go into the Application menu 1.7
  • Enter Stop configuration
  • Enter " type of stop"
  • Change SST (type of stop) value to NST and enter.
Additional  resources (attached):  ATV71 programming manual  and ATV61 programming manual.

type of stop

Schneider Electric Nigeria

Attachment(s)
ATV61_Programming_manual_EN_1760649_09.pdf [2.37 MB]
ATV71_Programming_manual_EN_1755855_10.pdf [5.94 MB]