{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How does the EcoAisle accommodate lighting without interfering with the ceiling panels.

Issue:
How does the EcoAisle accommodate lighting without interfering with the ceiling panels.

Product line:
EcoAisle.

Environment:
Only ACRC100, ACRC301S, EcoBreeze .

Cause:
Install

Resolution:

•         Many datacenters are planned around the floor tiles, but planning also needs to happen for the illumination of the aisles between the rows of racks.  There are times that the layout may change and cause the lighting to not be directly above the aisle.  Deploying a ceiling panel containment system could block some of the lighting as well.  The EcoAisle system provides an integrated light mounting system that will provide additional illumination to the aisle.  This lighting system is constructed of long lasting energy efficient LED lighting that is controlled by a series of motion sensors.  There is also a manual switch provided with the system that will allow a user to turn the lights off when exiting the aisle as an extra level of control and energy conservation.

High Efficiency LED kits

Installation of the light kits and wire routing is integrated into the extrusion  of the ceiling panel support rails

On/off Motion Sensors with manual over ride switch.

Schneider Electric Nigeria