{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is meant by thermal current rating (Ith) for Contactor "D" or "F" type ?

It means the rated current that this contactor can switch for Load category AC1 (thermal loads),

Example: LC1D09 is 9 A on AC3 and its thermal current (Ith = 20 to 25 A) (this means it can switch up to 20 or 25 A for loads of AC1

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: