{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the NetShelter CX integral PDU be replaced, or can another be added if a dual power input is required for redundancy? Which PDU comes in the CX?

Issue:
Need an additional or replacement PDU in the NetShelter CX.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Additional PDU or replacement necessary

Resolution:
Yes, the PDU can be replaced or others can be added.
The original PDU included with the cabinet is the APC part number AP9568 for EMEA cabinets (50Hz), and AP9567 for  NEMA cabinets (60Hz).

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: