{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What sort of equipment can be deployed in a NetShelter CX?
Issue:
What kind of equipment can be installed into the NetShelter CX?

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Customers want to make sure that their equipment can be installed into the cabinet.

Resolution:
Rack mount or tower servers, with associated UPS, switches, routers and distribution/patch panels. Communications or audio visual equipment.

Note: the number of servers and other heat generating devices is limited by their combined power ratings. A fully loaded cabinet will likely consist of servers and networking equipment.

Schneider Electric Nigeria