{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How much extra space is there to the front and rear of the internal rack posts on the NetShelter CX when the rails are at their furthest positions?

Article available in these languages: Russian

Issue:
Customers need to know how much room there is in the NetShelter CX beyond the rails.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Customers want to avoid interference with the front door and rear fan units.

Resolution:
Forward of the front rack posts = 100mm / 4”
Rearward of the rear rack posts = 60mm / 2” (Except, where fan modules intrude there is no usable extra space)

Schneider Electric Nigeria