{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
The NetShelter CX doors are not aligned. Can they be adjusted?
Issue:
NetShelter CX Door Misalignment

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
The cause for an uneven door may not be known but it can be corrected.

Resolution:
Make sure the floor is even and, if not, adjust the leveling feet and level the cabinet.
Also, the doors may move slightly in transit. If this happens the hinges can easily be adjusted to fix this. Use a phillips head screwdriver to move the hinge as required.

Schneider Electric Nigeria