{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Altivar drive is showing dCb on the display.
Issue:
What is the error code dCb on the Altivar Drive's display.
Product line:
Altivar drive families: ATV12, ATV28,  ATV312, ATV32, ATV61, ATV71.
Environment:
All models, all serial numbers.
Cause:
DC Injection Braking.
Resolution:
This is a normal drive state.  It is indicating the drive is injecting DC current into the motor to slow the motor down.  This typically appears on deceleration or at the end of the deceleration ramp.  On some drives, DC Injection can be turned on using a Logic Input.

Schneider Electric Nigeria