{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I replace an ATV21 drive in an SFLEX with a ATV212 drive?
Issue:
Replace an ATV21 S-Flex Drive.

Product Line:
Altivar 21 ATV21

Environment:
All models, All series

Cause:
Inoperative ATV21 drive in an SFLEX enclosure. Need to replace the ATV21 power converter.

Resolution:
Yes, you can replace the ATV21 drive with a ATV212 (same size)  drive inside the S-FLEX enclosure.

Schneider Electric Nigeria