{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How do you wire the ATS22 with S6U suffix, for 2-wire control?

Issue:
Wiring the ATS22 with S6U suffix, for 2-wire control.

.Product Line:
Altistart 22

Environment:
All Altistart 22's ending with S6U suffix (120V)

Cause:
Basic wiring examples

Resolution:

IFrame

The S6U requires constant 120VAC to terminals CL1 (hot) and CL2 (neutral).

For a freewheel stop:
Connect a jumper from Terminal LI1 to LI2.
Connect a jumper from Terminal CL2 to COM.
Close a dry contact between Terminals CL1 and LI2 for a run forward.  Open this connection for a freewheel stop.


For a controlled stop:
Do not jumper LI1 to LI2, wire LI1 to CL1, use run contact between CL1 and LI2, and program SEt - dEC = ramp down time.
diagram


Note: The factory default setting for the dEC parameter is 'free'. Leaving this parameter set to 'free' will provide a freewheel stop, regardless of which way LI1 and LI2 are wired. (This is why the Quick Start Guide shows a wiring diagram similar to the one above and indicates that it allows a freewheel stop.) Conversely, removing voltage from LI1 will result in a freewheel stop, regardless of the value set for dEC. In other words, a freewheel stop can be accomplished by wiring and/or programming.


Refer to the ATS22 User manual, ATS22 Quick Start Guide, or the Quick Start Annex for more information.

Schneider Electric Nigeria

Attachment(s)
ats22_user_manual_en_bbv51330_02 2 wire control.pdf [47.44 KB]