{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What causes an OPF1 fault on the ATV61 or ATV71 drives?

Issue:
OPF1 on ATV61/ATV71 drives.

Product Line:
Altivar ATV61 and ATV71

Environment:
All ATV61 and ATV71 drives

Cause:
1 phase loss between the drive and motor.

Resolution:
This fault is triggered when the drive detects one of the motor phases has been lost (or has very low current) for more than 500 msec.

Troubleshooting steps:

  • Check all connections between the drive and the motor. Re-seat connections and check for torque.
  • Using clamp-on measure current on each motor lead to see if you have low current on one or more phases.
  • Using a 1000 V Megger, test the motor and leads.
  • For testing, set Motor Control Type = VF2pts, Output Phase Loss = No, disconnect the motor leads from the drive, run the drive at 20Hz, 40Hz, and 60Hz, and measure output voltage phase to phase at each speed. You want the voltages balanced and correct for the speed you're running the drive. Be aware that your meter may read higher output voltage than you might expect (for example, you may measure over 500V at 60Hz) if your meter doesn't have a PWM filter. This is because you're measuring a PWM (Pulse Width Modulated) waveform and not true AC. Be sure to turn OPL detection back on after testing.
  • Go to 1.8 menu: Scroll down to Output Phase loss- Output time detect- set to 5 secs.  Power cycle the drive and then try to run again.

Schneider Electric Nigeria