{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What would cause an EPF2 fault on the ATV61 drive with an Ethernet IP card?

Issue:
What would cause an EPF2 fault on the ATV61 drive with an Ethernet IP card?

Product Line:
Altivar ATV61

Environment:
All

Cause:
Using an Allen Bradley PLC trying to access assemblies 103 and 104, and the drive has not been set up per case 2 example as recommended in the Ethernet IP VW3A3316 manual.

Resolution:
Case 2 programming example is as follows:

  • Menu 1.6
  • Ref 1= Communications card
  • Profile= Separate controls
  • CMD switching= C312
  • CMD channel 1= Communication card
  • CMD channel 2= Terminal control
  • Ref 2 Switching= C313
  • Ref 2 Channel= AI1 or AI2

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: