Search FAQs
How can I monitor the logic inputs status in Ethernet TCP/IP for ATV61 and ATV71 ?
Issue:
Monitoring the logic input map to determine status of the logic inputs.
Product Line:
Altivar 61/71
Environment:
All Models and serial numbers. Ethernet IP with Assemblies 100 and 101 with Profile as I/O
Cause:
None
Resolution:
To monitor the state of the logic inputs add logic address 5202 in the input scanner. This is a read only and allows monitoring of the logic input map. The map is as follows.
Bit 0 is LI1
Bit 1 is LI2
Bit 2 is LI3
Bit 3 is LI4
Bit 4 is LI5
Bit 5 is LI6
Monitoring the logic input map to determine status of the logic inputs.
Product Line:
Altivar 61/71
Environment:
All Models and serial numbers. Ethernet IP with Assemblies 100 and 101 with Profile as I/O
Cause:
None
Resolution:
To monitor the state of the logic inputs add logic address 5202 in the input scanner. This is a read only and allows monitoring of the logic input map. The map is as follows.
Bit 0 is LI1
Bit 1 is LI2
Bit 2 is LI3
Bit 3 is LI4
Bit 4 is LI5
Bit 5 is LI6
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: