{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum distance the motor can be from the ATV61 and ATV71 drive?


Issue:
is there a maximum distance of the cables connected between the drive and motor?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Application notes on motor cable distance.

Resolution:
Length of motor cables from ATV61


Length of motor cables from ATV71

Length of motor cables from ATV71
Length of motor cables from ATV71

Schneider Electric Nigeria