{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the ACSC fan system fault tolerant?
Issue:
Is the ACSC fan system fault tolerant?

Product line:
ACSC100, ACSC101

Environment:
InRow Cooling

Cause:

Resolution:
Yes, there are 2 power supplies in the unit for the condenser and evaporator fans. If 1 fails the other can supply 70% of the maximum power needed, so maximum fan capacity would be reduced approximately 30%. A user can replace the failed power supply from the front of the unit while the ACSC is still in operation. The evaporator fans are also hot swappable.

Schneider Electric Nigeria