{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is capacity regulation on an ACRD?

Issue:
What is capacity regulation on an ACRD?

Product line:
ACRD100, ACRD101, ACRD200, ACRD201

Environment:
Data Center Cooling

Cause:

Resolution:
Capacity regulation is a method of controlling the capacity of the InRow ACRD unit. This is achieved using an electronic Hot Gas Bypass Valve (HGBV) which allows the unit to operate at low load conditions down to 2.5 KW without compressor recycling.

Schneider Electric Nigeria