{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
With VM Startup enabled, PowerChute Network Shutdown Fails to Restart a Fault Tolerant VM that it shut down.
Issue:
In addition to the Fault Tolerant VM failing to start, there are errors reported in the vSphere client for PowerChute Network Shutdown (PowerChute) attempting to start a secondary VM.

Product Line:
PowerChute Network Shutdown v3.1, 4.x, 5.x

Environment:
VMware

Cause:
This issue occurs if the vCenter Server goes offline during a shutdown sequence. PowerChute then fails to identify which VM is the primary and which is the secondary.

Resolution:
None. When the vCenter Server becomes accessible, PowerChute will be able to identify the primary VM and issue a startup command to it. The system will start the secondary VM.

Schneider Electric Nigeria