Issue:
Upgrading the firmware on the ATV71 and ATV61 drives.
Product Line:
ATV61, ATV71
Environment:
All models and serial numbers
Cause:
Firmware update
Resolution:
The control board can be sent into the Schneider Electric Industrial Repair Center for upgrading the firmware to the latest level. Check with your local distributor for details.
Also, you can order a new replacement main control board part number:
VX4A61100Y ATV61 frame sizes 1 thru 9
VX4A71100Y ATV71 frame sizes 1 thru 9
VX4A61101Y ATV61 frame sizes 10 thru 16
VX4A71101Y ATV71 frame sizes 10 thru 16
Released for:Schneider Electric Nigeria