Issue:
Customer needs to know which S-flex 212 drives have a fusible disconnect or circuit breaker?
Product Line:
ATV212 S-Flex
Environment:
ATV212 (1 hp-100 hp S-Flex)
Cause:
Which enclosed units have fuses and which come with circuit breakers?
Resolution:
All of the S-Flex drives will have circuit breakers for short circuit protection except the 460VAC 75HP, 100HP SFD212RG4 and SFD212SG4. These two will have a fusible disconnect.
Note: All of the 460VAC units will have power fuses and circuit breakers except the 75HP and 100HP that will not have the circuit breaker but only fuses.
Released for:Schneider Electric Nigeria