{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum duty cycle of the braking transistor of the ATV32 series drives?
Issue:
Does Schneider Electric list the ATV32 maximum duty cycle of the braking transistor?

Product Line:
Altivar 32

Environment:
All models, All serial numbers.

Cause:
Application requiring a braking transistor's continuous use

Resolution:
The braking transistor in the ATV32 series drives is designed to handle Nominal motor power continuously and 150% of nominal motor power for 60 seconds.
An appropriately sized braking resistor must be used that is also capable of handling the required duty cycle.

Schneider Electric Nigeria