Issue:
Customers require information on grounding NetShelter cabinets to IEC specifications.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
This installation requires grounding per IEC specifications.
Resolution :
NetShelter SX cabinets are UL Listed and have all metal components grounded per UL/IEC 60950 requirements and meet the 0.1 ohm resistance.
Equipment to be installed in a NetShelter SX cabinet should be Listed equipment.
Installation of any unlisted or recognized components requires a safety review of the completed assembly.
Customers require information on grounding NetShelter cabinets to IEC specifications.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
This installation requires grounding per IEC specifications.
Resolution :
NetShelter SX cabinets are UL Listed and have all metal components grounded per UL/IEC 60950 requirements and meet the 0.1 ohm resistance.
Equipment to be installed in a NetShelter SX cabinet should be Listed equipment.
Installation of any unlisted or recognized components requires a safety review of the completed assembly.
Released for:Schneider Electric Nigeria