{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Sepam Main/Feeder Application Notes

Issue
What is the difference between the ANSI Main/Feeder - IEC Feeder and IEC Main

Product Line
Sepam 20
Sepam 40
Sepam 50
Sepam 60
Sepam 80

Resolution
Here is an overview of the attachment below.  For more information please open attachment.

ANSI and IEC Main Breakers are wired differently. ANSI standard wiring practices have CT polarity orientation towards the source of power, where IEC standards has the CT polarity orientation toward the switchgear bus. See Figure 1. Therefore, for IEC main breaker applications, the normal flow of power is into the non-polarity side of the cts. The manufacturing advantage of the IEC switchgear is that the IEC main and feeder are identical. In switchgear constructed per ANSI standards the CT polarity is towards the source for both the Main and the Feeders. IEC and ANSI feeders are the same.

Schneider Electric Nigeria

Attachment(s)
MAIN_FDR_APP_Note.zip [505.13 KB]