{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum current value which can go through CSH30 primary (P1-P2)?

Product Line
CSH30

Resolution
Withstanding characteristics of CSH30 are:

Continuous overload : 300 A primary
1 second overload : 12.5kA primary
Limiting dynamic value : 32kA peak (one time)

Within these limits Sepam will continue to work properly.

Schneider Electric Nigeria