{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Sepam series 80 cycle time?

The software embedded in Sepam series 80 (firmware) operates cyclically and deterministically. The cycle time is the time that it takes the Sepam series 80 to perform all of the «fast» functions. During a fixed cycle time of 14 ms, the system performs the self-tests, protection functions, logic input updating, control logic and equation editor, logic output updating and a portion of the slow functions (measurements).

Re-published to revised security level: 18 June 2008 by DRM

Applies To: Sepam Series 80

Public

All content © 1992-2008 Schneider Electric

Schneider Electric Nigeria