{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Sepam 1000+ and ACE990 - Io setting point in Amperes only


It is not possible to set the Io value differently than by whole numbers in Amps in case of use of an ACE 990 adapter. The consequence of this is naturally that one cannot specify a value of precision for low values of Io. It is recommended to simply choose the nearest and the most judicious whole number in the function of the electrical network.

Re-published to revised security level: 17 June 2008 by DRM

Applies To: ACE990 version v1.0

Original Author: (recommended to place initials only)

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166625 V2.0, Originally authored by LaVI on 06/20/2008, Last Edited by DaMi on 06/20/2008
Related ranges: Sepam series 40, ACE 9XX, Sepam series 20

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.