{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
With Sepam series 80 devices that use 2 sets of current APS_SENSORS, is it possible to use one set of LPCT APS_SENSORS and one set of In/5A or In/1A APS_SENSORS ?

Yes, with Sepam series 80 devices that use 2 sets of APS_SENSORS, it is possible to connect conventional current APS_SENSORS (In/5A or In/1A) and/or LPCT APS_SENSORS.
It is only with Sepam series 80 devices that use transformer differential protection (Sepam T87, M88 and G88) that LPCT APS_SENSORS may not be used.

Re-published to revised security level: 17 June 2008 by DRM

Applies To: Sepam 1000+ (Sepam Series 20 and Sepam Series 40)

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166656 V2.0, Originally authored by LaVI on 06/18/2008, Last Edited by DaMi on 06/18/2008
Related ranges: Sepam series 80

Schneider Electric Nigeria