{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the SBO remote control transmission mode?

With the Modbus communication link, remote control orders such as opening and closing of the breaking device or activation/inhibition of Sepam functions can be transmitted to Sepam 1000+.
The remote control orders may be carried out in 2 modes:
- direct mode: the remote control order is effective as soon as it is received
- SBO, Select Before Operate mode: the remote control order is executed in 2 steps, after reception by Sepam of 2 coherent orders, first the selection order and then the execution order.

The SBO mode is safer.

Schneider Electric Nigeria