{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the I/O Expander’s Digital Inputs and Outputs function if the power supply is not connected?

In the I/O expander, only the Analog Outputs are excited by the internal power supply. Digital Inputs and Outputs are externally excited and powered from the meter itself. So, Digital Inputs and Outputs will work without the power supply being energized.

Last Revised: April 9, 2008
Applies To: ION 8600, I/O Expander
Original Author: KG
Public
All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL191645 V1.0, Originally authored by KBAdPM on 04/10/2008, Last Edited by KBAdPM on 04/10/2008
Related ranges: Cabling and connection accessories, ION8600

Schneider Electric Nigeria