{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to retrieve a fault recording (OPG) in SFT2841 from the Sepam Series 20, 40,60 and 80 Relay?

Issue
How to retrieve a disturbance recording from a Sepam relay using SFT2841.

Product Line
Sepam Series 80
Sepam Series 60
Sepam Series 40
Sepam Series 20
SFT2841

Resolution
Steps to retrieve fault recording in SFT2841: (Note: Screen Caps may appear differently depending on Sepam series)

1. Verify communication between PC and Sepam. This indicator is located on the bottom left-hand side of SFT2841 window.

Image 1

2. Click on "fault recording" located on the Menu bar.

Image 2

3. Select the desired waveform based on the date/time and then click on the "retrieve" button.

Image 3

4. Select the save location and click "save"

Image 4

5. SFT2841 will take some time to download the OPG (fault recording). After the download is complete, you can use WAVEWIN Data Management and Analysis System software or some other equivalent software to view the waveform capture.  Note that SFT2826 is obsolete and no longer available so use Wavewin instead.

Please see the following video for walk through instructions.

Schneider Electric Nigeria

Video: How to retrieve a fault recording (OPG) in SFT2841 from the Sepam Series 20, 40,60 and 80 Relay?

Issue
How to retrieve a disturbance recording from a Sepam relay using SFT2841.

Product Line
Sepam Series 80
Sepam Series 60
Sepam Series 40
Sepam Series 20
SFT2841

Resolution 
Steps to retrieve fault recording in SFT2841: (Note: Screen Caps may appear differently depending on Sepam series)

1. Verify communication between PC and Sepam. This indicator is located on the bottom left-hand side of SFT2841 window.

Image 1

2. Click on "fault recording" located on the Menu bar.

Image 2

3. Select the desired waveform based on the date/time and then click on the "retrieve" button.

Image 3

4. Select the save location and click "save"

Image 4

5. SFT2841 will take some time to download the OPG (fault recording). After the download is complete, you can use WAVEWIN Data Management and Analysis System software or some other equivalent software to view the waveform capture.  Note that SFT2826 is obsolete and no longer available so use Wavewin instead.  

Please see the following video for walk through instructions.

 

Schneider Electric Nigeria

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range: