{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the communication accessory ACE 850 compatible with Sepam 80?

YES. The Communication Accessory ACE 850 is compatible with the Sepam 80 if the Sepam 80 Base Version is greater than or equal to V6.01 and if TCP/IP option reference 59754 has been placed the order.

Note: The cable between Sepam 80 and its ACE 850 (CCA614 reference 59751) must be plugged in on the Sepam 80 F Port.

Schneider Electric Nigeria