{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is is possible to identify the Sepam product's application and hardware features from the labels on the left side panel of the base unit? (North America)

The labels located on the left side panel of the Sepam Series 20, 40 & 80 identify the relay's application and hardware features. The attached document provides information relating to these labels. Notice that the part numbers on these labels are SQ1XXXX. This means that the Sepam relay is sold in North America and are branded as a Square D Product. If the relays are sold outside of North America, the part numbers would include SP1XXXX.
labels.pdf

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.