Search FAQs
Where to download the latest version of SFT2841
Issue
Need the settings software for SEPAM 20, 40, 50, 60, and 80 series.
Product Line
SEPAM SFT2841
Environment
Configuration tool, settings software
Cause
Where to download the latest version of SFT2841
Resolution
Click here to download the latest version of SFT2841 v17.4
Note: for customer with the latest build of Windows 10, or newer OS.
When installing the software use your previous serial number
The install will not complete without a valid serial number. If this is your fist install of this software you will need to enter 0647740-08 as the serial number.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: