{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Configuring GOOSE in Easergy Studio (MiCOM S1 Studio)

Issue
Need to program the MiCOM relay for publishing and receiving GOOSE messaging.

Product Line
MiCOM Px4x
Easergy Studio

Environment
Programming using Easergy Studio (MiCOM S1 Studio)

Resolution
The objective of this tutorial is to illustrate the configuration of basic GOOSE messaging on two Px4x series IEDs. Once the configuration is complete pressing Function Key 1 on one IED will send a GOOSE signal to the second relay and illuminate LED #1 on that relay. Also, pressing Function Key 1 on the second IED will send a GOOSE signal to the first IED and illuminate LED #1 on that IED. In other words, one will setup IED_1 to publish a GOOSE message which is linked to the state of its Function Key 1. Also, one will setup IED_1 to subscribe to the GOOSE message that is published by IED_2 and have that message turn on or off IED_1s LED #1.

Follow the instructions provided in the attached tutorial document: S1 Studio 61850 tutorial.pdf

Schneider Electric Nigeria

Attachment(s)

S1_Studio_61850_tutorial.pdfS1_Studio_61850_tutorial.pdf [621.09 KB]