Search FAQs
What are the differences between ProWORX NXT and ProWORX NXT Lite?
Issue:
Differences between ProWORX NXT and ProWORX NXT Lite
Product Line:
ProWORX NXT
Resolution:
The ProWORX NXT Full and Lite packages have the same functionality. There are no differences/limitations between the two packages other than the PLCs they support.
372SPU68001NDEV .....ProWORX NXT full Offline/Online Development Package. Supports all of the Momentum, Quantum, 984 Series Slot Mount, Compact, Modicon Micro 110CPU,
Modicon Micro984, 984A,B,X Chassis Mount, Atrium and VME controllers.
372SPU61001NLDV .....ProWORX NXT Lite Offline/Online Development Package. Only supports the Momentum, Compact and Modicon Micro 110CPU controllers.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: