Issue
ProWORX 32 Server limitations
Product Line
ProWORX 32...All versions
Environment
Windows 7
Resolution
The following limitations have been found on the ProWORX 32 server.
- If the server is being used for communicating to the PLC:
connecting to the server for puts and gets at the same time that the clients
are connected to the PLC via the server.
- If the server is used only for project storage and retrieval (the server is not used for
No limitations on number of users simultaneously connected with
either Modbus Plus or TCP/IP other than what is allowed for the server PC's
Microsoft Windows operating system's TCP/IP connections and the Modbus Plus
Adapter card.
- Maximum number of users configured on the server:
- No limitations.
- Maximum number of projects stored on the server.
No limitations other than the hard drive free space capacity.
Released for:Schneider Electric Nigeria