{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How long does the Simulation Build run for with Vijeo Designer V6.2?

Issue:
Vijeo Designer simulation running time

Product Line:
Vijeo Designer

Environment:
HMI Configuration Software

Resolution:
The simulation build in Vijeo Designer V6.2 runs for up to 1 hours.
It must be restarted to get another hour..

To run longer time a Vijeo Designer Runtime license is required. The part number for the Runtime license are as follow:
VJDSNRTMPC --Vijeo Designer Runtime Magelis iPC for Runtime version 6.2 SP10 and below
VJDSNRTSPC ---Vijeo Designer Runtime Standard PC for Runtime version 6.2 SP10 and below

The 4 new part numbers for Vijeo Designer V6.2 SP11 and above Runtime are as follows:

1) VJDRPCCZLSPMZZ – Vijeo Designer Runtime Standard PC – Printed
2) VJDRPCCZLSPAZZ - Vijeo Designer Runtime Standard PC  – Emailed

Licenses 1 and 2 support:
Generic PC
Harmony P6
Harmony iPC except box PC HMIBMP
Harmony iPC except box PC HMIBMU
Harmony iPC except panel PC HMIPSO
Harmony iPC except panel PC HMIPSP
Harmony iPC except panel PC HMIPEP

3) VJDHPCCZLSPMZZ – Vijeo Designer Runtime Harmony PC  - Printed
4) VJDHPCCZLSPAZZ - Vijeo Designer Runtime Harmony PC  - Emailed

Licenses 3 and 4 support:
Harmony iPC box PC HMIBMP
Harmony iPC box PC HMIBMU
Harmony iPC panel PC HMIPSO
Harmony iPC panel PC HMIPSP
Harmony iPC panel PC HMIPEP

Schneider Electric Nigeria