Search FAQs
Which Magelis XBTGT terminals has ATEX Certification for GAS?
Issue:
Magelis XBTGT terminals that has ATEX Certification for GAS
Product Line:
Magelis, XBTGT
Resolution:
Below are the Magelis XBTGT terminals that are ATEX Certified for GAS:
- XBTGT1000 Series
- XBTGT2000 Series
- XBTGT4000 Series
- XBTGT5000 Series
Please note that the XBTGT6000 and GT7000 series are not rated for GAS. Attached is the ATEX Certification document.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: