{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you add more then one Alarm Group to the Alarm Banner or Alarm Summary in Vijeo Designer?

In the Vijeo Designer Navigator right click on the Alarms and select "New Alarm Category"
image

Then add the Alarm Groups you want to display in the Alarm Banner or Alarm Summary,
Now Click OK
image2

Go to your Alarm Summary Settings or Alarm Banner Settings by double clicking on the Alarm Object on your Panel.
Then Select the Alarm Category instead of the Alarm Group. Then Click OK
image3

This Alarm Banner or Alarm Summary will now show the alarms from the Alarm Category you added to the Alarm display.

Schneider Electric Nigeria